Question
Hello, I had developed one application using STVD
Posted on March 25, 2017 at 10:03
#include 'Filter.h'
#define Samples 3#include <math.h>#include <stdlib.h>extern unsigned long int data;
long int Result_Previous,Average,;unsigned char Stable;void FIR_Filter(unsigned long int Clean)
{ static unsigned char Index=0;// static bit_16 Index1=4000; static unsigned long int ADC_Mean[Samples]; unsigned long int Absolute; unsigned char Count;// Average = Clean>>5; Clean >>= 5; ADC_Mean[Index] = Clean; Average = 0; { for(Count=0;Count<Samples;Count++) { Average+=ADC_Mean[Count]; } Average /= Samples; }if(Index >= (Samples-1))
Index=0; else Index++; Absolute = abs(Average - Result_Previous); if(Absolute <5) { Average = Result_Previous +((Average - Result_Previous)>>2); } if(Absolute<3) Stable++; else Stable=0; Result_Previous = Average;// return (Average); data = Average;}this is my code in interrupt function.. i think problem with this statement addition in variable not working in interrupt function ' Average+=ADC_Mean[Count];'
how can addition in that variable??
Help me for this.. Thank you..