Skip to main content
Visitor II
October 27, 2021
Question

Interrupt Handler execute issue on NUCLEO-8S208RB

  • October 27, 2021
  • 0 replies
  • 649 views

I downloaded the blink LED demo from ST and loaded in that nucleo board to check out how things worked, soon I found out that every time when I pressed the "USER" Button (Connected to PE4), It won't be able to successfully switch to next blink pattern 100%, It sometimes would fail to switch over. I thought it maybe was a bad button issue but I debugged with IDE inserts a few breakpoint into the codes and I found some interesting behavior from the Interrupt Handler:

Related Code as follows:

NTERRUPT_HANDLER(EXTI_PORTE_IRQHandler, 7)
{
 /* In order to detect unexpected events during development,
 it is recommended to set a breakpoint on the following instruction.
 */
#if defined(USE_STM8S_NUCLEO_64)
 if(BlinkSpeed == 3)
 {
 BlinkSpeed = 0;
 }
 else
 {
 BlinkSpeed ++;
 }
#endif /* USE_STM8S_NUCLEO_64 */
}

It just a simple code for switching modes, If I insert breakpoints in line 7,9 and 10 and execute line by line in debug mode, it work out perfectly, switching blink pattern every time I pressed the button. But if I take off all the breakpoints or when 7 or 9 then it will start acting glitchy. What caused this issue and how to solve this?

    This topic has been closed for replies.