Skip to main content
Visitor II
January 15, 2010
Question

Linker errors while compiling any of sample project in STVD

  • January 15, 2010
  • 5 replies
  • 1629 views
Posted on January 15, 2010 at 19:09

Linker errors while compiling any of sample project in STVD

    This topic has been closed for replies.

    5 replies

    kamil23Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:06

    Hello,

    I am looking for some help with the following issue:

    Running Linker

    clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib'' -o Debug\discover.sm8 -mDebug\discover.map Debug\discover.lkf

    #error clnk Debug\discover.lkf:27 can't open file crtsi0.sm8

    #error clnk Debug\discover.lkf:47 can't open file libis0.sm8

    #error clnk Debug\discover.lkf:48 can't open file libm0.sm8

    The command: ''clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib'' -o Debug\discover.sm8 -mDebug\discover.map Debug\discover.lkf '' has failed, the returned value is: 1

    exit code=1.

    discover.elf - 5 error(s), 0 warning(s)

    Same thing while trying to build ADC sample.

    Help much appreciated.

    Thank you!

    kamil23Author
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:06

    Thank you mozra,

    It appears that for some reason all of my tool paths contained a series of non alfanumeric characters at the end.

    I was able to copy the setting from my colleague.

    Many thanks!

    Kamil

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:06

    Well, whenever something says that it ''can't open'' a file, you have to ask yourself why - don't you?

    Have you checked that these files exist on your PC?

    If they do exist, have you checked that the tools are correctly configured to find them?

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:06

    Hi,

    you can update your cosmic path(Tools>Options>Toolset>Root path) as following C:\Program Files\COSMIC\CXSTM8_16K (remove Lib directory from the path)

    Regards

    mozra

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:06

    Hi mozra27,

    it seems this is a bug of latest STVD version:

    STVD MainFrame Version 3.6.4.2 - Build Dec 17 2009

    stvabbld.dll, Version: 1.3.3.0

    stv7abbld.dll, Version: 1.4.3.0

    STVD_TxtEditor.dll, Version: 1.0.2.5

    addonide.ini, Version: Rel 4.0, Date: 19 February 2008

    ProgrammerAddOn.dll, Version: 1.3.0.1

    st7expor.dll, Version: 3.3.4.0

    when migrating on this new version I had the same problem: I had to specify manually root path for Cosmic, and it was not the case before.

    brazov2