Question
Maximal toggling frequency of STM8
Posted on October 07, 2016 at 15:06
Hi,
I have just started with STM8 and would like to found the fastest toggling method.Currently I have best result with following code: while (1) {#pragma asm push A pushw X ld A, #1 // toggle with pin D0 ldw X, #0x500f // GPIOD (port D output latch) clr (X) ld (X), A clr (X) ld (X), A clr (X) ld (X), A clr (X) ld (X), A clr (X) ld (X), A clr (X) ld (X), A popw X pop A#pragma endasm }The block of 6x CLR / LD makes ''bit clear'' / ''bit set''.Size of both instructions is 1 byte, so fetching shouldn't cause any delay.The result is Low 62.5ns / High 125ns (i.e. 1c/2c @16MHz), repeating 6x.I don't understand why the 1c/1c toggling is not achieved.I would like to ask for explanation of this and solution for 1c/1c toggling (if possible).Thanks