Posted on May 17, 2011 at 15:10 Thank you on that....but how can i use PA as USART, cause it uses PC, no port remaping option but it was indicated at datasheet that it can be use...
Posted on May 17, 2011 at 15:10 Sorry was not that clear. i mean, its default port use was PC2/[USART1_RX](3)/LCD_SEG22/ADC1_IN6/COMP1_INP/VREF_OUT and PC3/[USART1_TX](3)/LCD_SEG23(2)/ADC1_IN5/COMP1_INP/COMP2_INM and in my application I want to use this as my USART PA2/OSC_IN/[USART1_TX](3)/[SPI1_MISO] (3) and PA3/OSC_OUT/[USART1_RX](3)/[SPI1_MOSI](