Question
Power Consumption with Input NOT at Rail
Posted on February 02, 2016 at 23:22
I am using the STM8S103K3. The data specifies power consumption only with all inputs at the rail voltage. Also the data sheet says to ''turn off schmitt input'' on adc input to save power. These things imply that excess power is consumed by digital inputs when not at the supply rails.
My PWM outputs are tied to Vcc/2. When I turn them off how much power will be consumed by the input being at Vcc/2. If I drive the output to one of the rails this will also consume power. So I have to choose one or the other ... or add circuitry.