Problem in displaying a number on char LCD displays
Hi.
I was working with my new stm8s105 MCU trying to get started with the timers.
But every time I use the command to display the time on the LCD the same number showed every time.I thought that the problem is my timer code but when I just put a number on the LCD to show it just showed an irrelevant number.
I use the same LCD.h on LPC1768 and STM32F2 and just converted the same header.The only difference is that I used Keil compiler for them and now I'm using IAR.
lcd_gotoxy(1,2);
sprintf(buf,'%d',100);lcd_print(buf);delay_ms(1000);This is a simple code that must show 100 but it displays 12594
>:(
The characters are displayed properly.The problem is numbers.