Question
query regarding the value of the Vcap in STM8S microcontroller
Posted on May 29, 2012 at 09:18
Hello sir
I am using the STM8S103F2P6 microcontroller of the ST microelectronics and when I was studying the power supply section of the microcontroller there it is specified to connect an external capacitor with the value ranging in between the 470 to 3300 nf . the specifications for the external VCAP capacitor are as follows:Value = 470 to 3300 nfESL = 15 nH max.ESR = .3 ohm at 1 MHz.But I have connected the 1 uF value capacitor to the Vcap pin of the microcontroller , because I was not getting the microcontroller of that range .So I want to know that is it ok , or it is going to effect my microcontroller in any way. I mean what will be the effect and how it will effect my whole circuit and the microcontroller.Please describe me in detail.Thank you