Simple wiring of STM8S003F3P6TR for one input and one output
Greetings
I'm using an STM8S003F3 TSSOP20 (my first STMicro) for a simple project with one input (low frequency PWM) and one output (high frequency PWM). I seek to keep it as simple as possible. Since I'm not familiar with STMicro MCU's, I would like to confirm the wiring of this:
100nF between NRST and VSS
1uF between VCAP and VSS
1uF and 100nF in parallell between VDD and VSS
+5V to VDD
0V to VSS
VDD, VSS, NRST and SWIM connected to ICSP plug.
PWM input on PD2
PWM output on PD3
All other pins connected together, with one configured as output, driven to 0V
Thanks in advance for any helpful advice!