SM8S105 Flash Image(please help urgent)
Hi
I am designing my code using the STM8S Discovery.
When using the Cosmic compiler i get the following files generated after compiling(no debug).
stvd_project_dtd416.elf (29KB)
stvd_project_dtd416.lkf (3KB)
stvd_project_dtd416.s19 (27KB)
stvd_project_dtd416.sm8 (31KB)
Which of the above images is actually written to flash. I am implementing a ICP using SWIM which will write the actual image directly to flash program memory so i need to know which image to write.
Need help urgently.
Thanks