Some GPIOs in the STM8S003FS isn't working in the normal PP_OUT mode
Hello,
I'm working on a project in which I want to generate some trigger output ( which is connected to a sound chip APR33A3). Hence, I'm using the controller STM8S003FS GPIOs to generate the trigger output. Unfortunately, for an unknown reason, some of the GPIOs are not working properly in the normal push-pull out mode. I've marked them in the Image attached below. The output of these GPIOs is staying unchanged (checked physically via multi-meter).
I'm also adding the snippet of my code, so, if I made any mistake please let me know.
The nor working pins are as follows:
- PA3 (HS)/[SPI_NSS] TIM2_CH3
- PD3 (HS)/AIN4/TIM2_CH2/ADC_ETR
- PD4 (HS)/UART1_CK/TIM2_CH1/BEEP
/* Includes ------------------------------------------------------------------*/
#include "stm8s.h"
#include "stm8s_conf.h"
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <intrinsics.h>
/* GLOBAL DEFINITION ----------------------------------------------------------*/
#define _KEY_0_PORT ( GPIOD )
#define _KEY_0_PIN ( GPIO_PIN_2 )
#define _KEY_1_PORT ( GPIOD )
#define _KEY_1_PIN ( GPIO_PIN_3 )
// #define _KEY_1_PORT ( GPIOA )
// #define _KEY_1_PIN ( GPIO_PIN_3 )
// #define _KEY_1_PORT ( GPIOD )
// #define _KEY_1_PIN ( GPIO_PIN_4 )
#define _KEY_2_PORT ( GPIOC )
#define _KEY_2_PIN ( GPIO_PIN_3 )
#define _KEY_3_PORT ( GPIOC )
#define _KEY_3_PIN ( GPIO_PIN_4 )
#define _KEY_4_PORT ( GPIOC )
#define _KEY_4_PIN ( GPIO_PIN_5 )
#define _KEY_5_PORT ( GPIOC )
#define _KEY_5_PIN ( GPIO_PIN_6 )
#define _KEY_6_PORT ( GPIOC )
#define _KEY_6_PIN ( GPIO_PIN_7 )
/* GLOBAL VARIABLE ------------------------------------------------------------*/
ErrorStatus enClkInitstatus = ERROR;
FlagStatus enClkSetStatus = RESET;
uint32_t ucClkFrequency = RESET;
/* FUNCTION DEFINITION --------------------------------------------------------*/
/**
* @brief FnCLKinit program.
* @param None
* @retval None
*/
void FnCLKinit (void)
{
/* CLK Deinit */
CLK_DeInit( );
/* Configure the HSI prescaler to the optimal value */
CLK_SYSCLKConfig( CLK_PRESCALER_HSIDIV1 );
CLK_HSIPrescalerConfig( CLK_PRESCALER_HSIDIV1 );
/* Configure the system clock to use HSI clock source and to run at 16Mhz */
enClkInitstatus = CLK_ClockSwitchConfig( CLK_SWITCHMODE_AUTO, CLK_SOURCE_HSI,
DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);
if(enClkInitstatus == ERROR) while(SET){ };
/* Enable the HSI*/
CLK_HSICmd( ENABLE );
ucClkFrequency = CLK_GetClockFreq( );
while ( (enClkSetStatus = CLK_GetFlagStatus(CLK_FLAG_HSIRDY)) != SET ){ } ;
}
/* FUNCTION DEFINITION --------------------------------------------------------*/
/**
* @brief FnGPIOValueWrite
* @param
* @retval None
*/
void FnGPIOValueWrite(GPIO_TypeDef* GPIOx, GPIO_Pin_TypeDef PortPins,BitStatus bitst)
{
if ( bitst == SET )
GPIOx->ODR |= (uint8_t)PortPins;
else GPIOx->ODR &= (uint8_t)(~PortPins);
}
/* FUNCTION DEFINITION --------------------------------------------------------*/
/**
* @brief FnUsart1Send
* @param ucData
* @retval None
*/
void FnUsart1Send(char *ucData)
{
uint16_t ucCnt = RESET ;
while (ucData[ucCnt] != NULL )
{
/* Write a character to the UART1 */
UART1_SendData8(ucData[ucCnt]);
/* Loop until the end of transmission */
while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET);
/* Increament the counter */
ucCnt++;
}
}
/* FUNCTION DEFINITION --------------------------------------------------------*/
/**
* @brief Main program.
* @param None
* @retval None
*/
int main()
{
/* Configure the */
FnCLKinit();
GPIO_DeInit(GPIOA);
GPIO_DeInit(GPIOB);
GPIO_DeInit(GPIOC);
GPIO_DeInit(GPIOD);
/* Initialize I/Os in Output Mode */
GPIO_Init( _KEY_0_PORT, _KEY_0_PIN, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_Init( _KEY_1_PORT, _KEY_1_PIN, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_Init( _KEY_2_PORT, _KEY_2_PIN, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_Init( _KEY_3_PORT, _KEY_3_PIN, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_Init( _KEY_4_PORT, _KEY_4_PIN, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_Init( _KEY_5_PORT, _KEY_5_PIN, GPIO_MODE_OUT_PP_HIGH_FAST);
GPIO_Init( _KEY_6_PORT, _KEY_6_PIN, GPIO_MODE_OUT_PP_HIGH_FAST);
FnGPIOValueWrite(_KEY_0_PORT,_KEY_0_PIN, RESET);
FnGPIOValueWrite(_KEY_1_PORT,_KEY_1_PIN, RESET);
FnGPIOValueWrite(_KEY_2_PORT,_KEY_2_PIN, RESET);
FnGPIOValueWrite(_KEY_3_PORT,_KEY_3_PIN, RESET);
FnGPIOValueWrite(_KEY_4_PORT,_KEY_4_PIN, RESET);
FnGPIOValueWrite(_KEY_5_PORT,_KEY_5_PIN, RESET);
FnGPIOValueWrite(_KEY_6_PORT,_KEY_6_PIN, RESET);
UART1_DeInit();
/* UART1 configuration ------------------------------------------------------*/
/* UART1 configured as follow:
- BaudRate = 115200 baud - Word Length = 8 Bits
- One Stop Bit - No parity
- Receive and transmit enabled
- UART1 Clock disabled
*/
UART1_Init((uint32_t)9600, UART1_WORDLENGTH_8D, UART1_STOPBITS_1,
UART1_PARITY_NO, UART1_SYNCMODE_CLOCK_DISABLE,
UART1_MODE_TXRX_ENABLE);
FnUsart1Send("TW_VOICE!\n\r");
while (SET)
{
}
}