Skip to main content
Visitor II
August 28, 2017
Question

SPI problems about STM8S103

  • August 28, 2017
  • 0 replies
  • 565 views
Posted on August 28, 2017 at 10:24

Good afternoon~everybody

I use STM8S103 to be the Slave device of SPI. However, I don

’

t know why all the interrupt of STM8 received is 0*1 instead of the right data? This is the

http://www.kynix.com/uploadfiles/pdf8798/STM8S103F2P3.pdf

and the code is as following:

[code]void spi_slave_init()

{

    //NSS

    GPIOA->DDR &= ~SPI_SSEL_PIN; //input pattern

    GPIOA->CR1 &= ~SPI_SSEL_PIN; //Floated input

    GPIOA->ODR &= (uint8_t)~SPI_SSEL_PIN; //write low

    GPIOC->DDR |= SPI_MISO_PIN; //

out

put pattern

    GPIOC->CR1 |= SPI_MISO_PIN; //

Push-pull output

    

    GPIOC->DDR &= ~SPI_MOSI_PIN; //

input pattern

    GPIOC->CR1 &= ~SPI_MOSI_PIN; //

Floated input

    

    GPIOC->DDR &= ~SPI_CLK_PIN;  //

input pattern

    GPIOC->CR1 &= ~SPI_CLK_PIN;  //

Floated input

    

        SPI_DeInit();        

        // Initialize SPI in Slave mode, NSS hardwere management  */

        SPI_Init(SPI_FIRSTBIT_MSB, SPI_BAUDRATEPRESCALER_2, SPI_MODE_SLAVE, SPI_CLOCKPOLARITY_HIGH, 

                SPI_CLOCKPHASE_2EDGE, SPI_DATADIRECTION_2LINES_FULLDUPLEX, SPI_NSS_SOFT,(uint8_t)0x07);

        SPI_ITConfig(SPI_IT_RXNE, ENABLE);// Receive buffer not empty interrupt Enable

        SPI_Cmd(ENABLE); // SPI enable

}

uint8_t spi_rw(uint8_t byte)

{

    char ch = 0;

    

    while (SPI_GetFlagStatus(SPI_FLAG_TXE) == RESET);

    SPI->DR = byte;

    while(SPI_GetFlagStatus(SPI_FLAG_RXNE) == RESET);

    ch = ((uint8_t)SPI->DR);

    

    return ch;

}

INTERRUPT_HANDLER(SPI_IRQHandler, 10)

{

  /* In order to detect unexpected events during development,

     it is recommended to set a breakpoint on the following instruction.

  */

  uint8_t Rx_byte; 

  Rx_byte = spi_rw(0x18);

  printf('%x ', Rx_byte)

:

}[/code[

Could anyboby here help me ? Thanks every much!

    This topic has been closed for replies.