ST-Link / V2 to program STM8S001J3 with STVP but not connect with the device
Hello, I'm using ST-Link / V2 to program STM8S001J3 with STVP (Swim connection). When I try to program MCU, the error appears that it was not possible to connect with the device. The pins are correct and I'm using 3.3V (Pin 19 to CN3 of ST-Link).
Even if there is an error, the led turns green after programming.
What is strange, I also use an STBM1008A for the same purpose and it works without problems.