Skip to main content
Visitor II
October 14, 2016
Question

ST Visual Develop Compile Error

  • October 14, 2016
  • 0 replies
  • 648 views
Posted on October 14, 2016 at 09:02

Hi,

I used the ST Visual Develop with Cosmic STM8 free tools with no limits version to compile a C program. However, some errors were shown,

''&sharperror clnk debug\stm8 gerenal io program.lkf:1 can't open file debug\stm8 gerenal io program.lkf

 The command: ''clnk -m ''debug\stm8 gerenal io program.map'' -l''C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Lib''  -o ''debug\stm8 gerenal io program.sm8'' ''debug\stm8 gerenal io program.lkf'' '' has failed, the returned value is: 1

exit code=1.''

Besides, the pop-up message box was shown ''Could not open the ''debug\stm8 file'' when I push ''Build'' button every time.

But I sure that

1) A License for the Cosmic was well installed because I already checked HKEY_CURRENT_USER->SOFTWARE->FLExlm License Manager-> COSMIC_LICENSE_FILE.

2)My C Program is small than 4k.

Please help. Thank you

#stvd-cosmic-compiler-stm8l
    This topic has been closed for replies.