Skip to main content
Visitor II
July 5, 2020
Question

STLINK-V3SET cannot communicate with target over SWIM (or doesn't work at all?) with STVD/STVP

  • July 5, 2020
  • 11 replies
  • 7277 views

I have an STLINK-V3SET with MB140B adapter.

I am trying to program an STM8S003F3P (minimum evaluation board) over SWIM

I've installed the en.stsw-link009 driver on my Windows10

I've put jumpers on JP4 and JP6

My code is specific for STM8S and compiled and builds fine.

When I use STVD or STVP to program the code on the chip, when pressing start I get the following:

Cannot communicate with the device, check the SWIM connection...

I tested continuity, everything is fine.

I actually think the STLINK-V3SET isn't working right!

When doing ST-LINK Upgrade, on Device Connect, I get: The content of the ST-Link is corrupt

I don't know if the ST-LINK Upgrade is just not compatible with the V3SET or my LINK is really broken...

How to start debugging my problem?

Thanks

    This topic has been closed for replies.

    11 replies

    Explorer
    November 18, 2020

    Be certain you are providing your Vcc on the 4 pin cable from your target.

    ST-Link needs this to to accept your targets signals.

    PS, next time this should be a new thread / question. G.H. <<<)))