STM*S-discovery with st8ms105c6t6 mcu -- I am going nuts
I have an asm program written in ST Visual develop. Using stvd, and updloading to a STMS103f3, it runs fine. Change the target in ST v develop and build it and upload to the discovery bd thru it's st-link, it doesn't run. Checking the register addr etc shows all the same, so it should work. Here is my code. I must be missing something to change between the boards or the built in st-link is the problem. It is attached so connecting my st-lin v2 or my ver 3 can't be connected without removing shorting links on it.