Question
STM8 Assembler using STVD with Assembler / Linker Toolchain
Posted on August 10, 2011 at 15:13
Further to a previous enquiry regarding ''The parameter is incorrect'' issue with STVD.
I've installed STVD V4.2.1 and Patch 2 but I'm still struggling with this problem of ''The parameter is incorrect'' on an ST8 application using the Assembler / Linker toolchain with STM8 Assembler code. I've tried to run the ST7 example 'realtime' supplied with STVD and this will not work either. With STM8 The system loads the mapping.asm and main.asm automatically and when a build is attempted the system reports ST Visual Develop The executable could not be found You can fix it by editing your toolset settings etc. etc. It hangs up while attempting to assemble mapping.asm and reports Error creating process for executable asm The parameter is incorrect Failed to create process. All files ie assembler, linker etc are located in a single project file and this is the path shown in project settings. What executable is it referring to? I am assuming it is the assembler executable. Any idea what's going on and how I can work round it? I'm running Windows XP on a fairly high spec machine. Thanks in anticipation of a solution. Regards