STM8 _block_cksum161
i used _blockcksum160 then we increase code size 32K to 64K
depends on code size increased;we changed memory model +modsl0 to modsl.We changed library list libislo.sm8;libmo.sm8 to libisl.sm8;libm.sm8We changed startup file crtsi0.sm8 to crtsi.sm8. When we run software, during runtime check. İt fails._block_checksum160() return CRC_ERROR. Then we start to use _block_checksum161() however, it return error;#error clnk Debug\canli.lkf:1 symbol _MSB_RunCrc16Chk not defined (Debug\_block_cksum161.o )#error clnk Debug\canli.lkf:1 symbol _MSB_RunCrc16ChkInv not defined (Debug\_block_cksum161.o )As i understand that stm8l_stl_classB_var.h ,which sent by ST guys, should update.
Where can be get
stm8l_stl_classB_var.h file which suit for 64K
stm8l_stl_classB_var.h :
#ifdef _COSMIC_
#pragma section @near [RUN_TIME_BUF] /* Buffer to store original RAM content during run-time tests */ EXTERN NEAR u8 RunTimeRamBuf[RT_RAM_BUF_SIZE];/* RAM pointers for run-time tests */
EXTERN NEAR u8 *p_RunTimeRamChk; EXTERN NEAR u8 *p_RunTimeRamChkInv;#ifdef STL_VERBOSE
EXTERN NEAR s16 FreqDifDisplay; /* Not really a Class B variable, but useful for debugging */ #endif /* STL_VERBOSE */ #pragma section @near [CLASS_B] EXTERN NEAR u16 MarchOverlayGap; /* gap in memory due to March test overlay */ EXTERN NEAR u16 CtrlFlowCnt; /* program flow execution at start */ EXTERN NEAR u8 LSI_HSIStartUpFreqkHz; /* First measure LSI over HSI stored */ EXTERN NEAR u8 LSI_HSEStartUpFreqkHz; /* First measure LSI over HSE stored */ EXTERN NEAR u16 LSI_StartUpPeriod; /* Initial measure of LSI - reference for run-time checks */EXTERN NEAR u16 LastCtrlFlowCnt; /* Control flow counter from one main loop to the other */
EXTERN NEAR const u8 *p_RunCrc16Chk; /* Pointer to FLASH for crc16 run-time tests */ EXTERN NEAR u16 CurrentCrc16; /* Current FLASH 16-bit Crc */ EXTERN NEAR u16 CurrentDesc; /* Current Descriptor Address */ EXTERN NEAR u8 CRCBlockIndex; /* Counter needed for partial CRC test */ EXTERN NEAR u16 MarchOverlayGap_; /* gap in memory due to March test overlay */ #pragma section @near [STACK_BOTTOM] /* Magic pattern for Stack overflow in this array */ EXTERN NEAR volatile u8 StackOverFlowPtrn[4];#pragma section @near [CLASS_B_REV]
EXTERN NEAR u16 MarchOverlayGapInv; EXTERN NEAR u16 CtrlFlowCntInv; EXTERN NEAR u8 LSI_HSIStartUpFreqkHzInv; EXTERN NEAR u8 LSI_HSEStartUpFreqkHzInv; EXTERN NEAR u16 LSI_StartUpPeriodInv; EXTERN NEAR u16 TickCounterInv; EXTERN NEAR u16 LastCtrlFlowCntInv; EXTERN NEAR const u8 *p_RunCrc16ChkInv; EXTERN NEAR u16 CurrentCrc16Inv; EXTERN NEAR u16 CurrentDescInv; EXTERN NEAR u8 CRCBlockIndexInv; EXTERN NEAR u16 MarchOverlayGapInv_;#endif /* _COSMIC_ */