STM8 CAN Filter
Hi,
I am working with the STM8AF5286UDY and am trying to set up a CAN interface.
For programming, I use the standard peripheral library. At the moment, my CAN interface works fine. The only thing, which does not work, is the filtering.
I use extended IDs and want to get all IDs from 0x18FEC100 to 0x18FEC999.
My code looks as follows:
/* CAN filter init */
CAN_FilterNumber = CAN_FilterNumber_0;
CAN_FilterActivation = ENABLE;
CAN_FilterMode = CAN_FilterMode_IdMask;
CAN_FilterScale = CAN_FilterScale_32Bit;
CAN_FilterID1=0x18FEC101;
CAN_FilterID2=0;
CAN_FilterID3=0;
CAN_FilterID4=0;
CAN_FilterIDMask1=0x1FFFF000;
CAN_FilterIDMask2=0;
CAN_FilterIDMask3=0;
CAN_FilterIDMask4=0;
CAN_FilterInit(CAN_FilterNumber, CAN_FilterActivation, CAN_FilterMode,
CAN_FilterScale,CAN_FilterID1, CAN_FilterID2, CAN_FilterID3,
CAN_FilterID4,CAN_FilterIDMask1, CAN_FilterIDMask2,
CAN_FilterIDMask3, CAN_FilterIDMask4);
I would apreciate any help! Thank you!