Skip to main content
Visitor II
March 23, 2009
Question

STM8_firmware_library

  • March 23, 2009
  • 15 replies
  • 5771 views
Posted on March 23, 2009 at 03:35

STM8_firmware_library

#can-init #stm8s-can-example
    This topic has been closed for replies.

    15 replies

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:01

    Thanks Olga,

    Your suggestion got me a step further but it didn't totally fix the problem I was having. I had created the project in one folder and then put the source files in a sub-folder of the project folder. When I built the project the compiler decided to un-include the stm8_interrupt_vector.c file that I had chosen from the sub-folder and it would then use the stm8_interrupt_vector.c file from the base project folder, which was actually for a different project. Lesson learned: create a seperate project folder for each project within a workspace!

    The project also needed your suggestion, so thanks for your help!

    Cam

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:01

    Just in case you want to leave the file in the sub-folder, you can change the stm8_interrupt_vector.c file throught this link:

    'Project'--> 'Settings'--> 'Linker'

    Select the category 'Input' and after select the vector file that you want.

    Regards,

    Olga

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:01

    Hello Everyone,

    I am new to STM microcontrollers and have started working with STM8/128 Eval board. I am experimenting with the CAN feature available with the Firmware library. But I am facing an issue with Initialisation of CAN controller. The function CAN_Config tries to Init the CAN controller by setting neccessary bits in CAN_MCR register but never comes out of the Init state and CAN Tx or Rx attempts there after. I wanted to check if some one has faced the same issue and was able to fix it.

    Regards,

    Achyut

    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 15:01

    I have a trivial question here.

    What directory structure would you recommend while using the examples from the firmware library?

    An example folder contains some source & header files. After creating a new project, peripheral specific source files and the library inc files are also required. So, any suggestions about how to maintain particular directory structure? Should some files be copied into new directories or should they be used from their current location?

    -SU

    [ This message was edited by: sandeep.undale on 23-03-2009 08:06 ]

    Visitor II
    July 23, 2012
    Posted on July 23, 2012 at 13:25

    how to check carry flag in stm8l