Question
Stm8 touch library
Posted on May 07, 2014 at 09:18
I intend to implement a single touch key using stm8 touch library. I am having few issues regarding this.
I haven't used the shield concept for noise immunity, so what does a need to define for : SCKEY_P2_DRIVEN_SHIELD_MASK in the configuration file.&sharpinclude''stm8s.h''&sharpinclude''stm8_tsl_api.h''&sharpdefine LED1_GPIO_PORT (GPIOB)&sharpdefine LED1_GPIO_PIN (GPIO_PIN_4)void main(){ LED1_GPIO_PORT->ODR |= (uint8_t)(LED1_GPIO_PIN); LED1_GPIO_PORT->DDR |= (uint8_t)(LED1_GPIO_PIN); LED1_GPIO_PORT->CR1 |= (uint8_t)(LED1_GPIO_PIN); LED1_GPIO_PORT->CR2 &= (uint8_t)(~(LED1_GPIO_PIN)); TSL_Init(); sSCKeyInfo[0].Setting.b.IMPLEMENTED = 1; sSCKeyInfo[0].Setting.b.ENABLED = 1; sSCKeyInfo[0].DxSGroup = 0x01; while(1) { TSL_Action(); if (sSCKeyInfo[0].Setting.b.DETECTED) { LED1_GPIO_PORT->ODR &= ~(uint8_t)(LED1_GPIO_PIN); } else { LED1_GPIO_PORT->ODR |= (uint8_t)(LED1_GPIO_PIN); } }}Also here is the main file code , I am not too clear about the validity of this code too. Please provide me help on this issue.Thank you. #stm8s-touch-sensing