stm8 tx by interrupt output many \0
INTERRUPT_HANDLER(USART1_TX_TIM5_UPD_OVF_TRG_BRK_IRQHandler,27)
{
/* In order to detect unexpected events during development,
it is recommended to set a breakpoint on the following instruction.
*/
USART_SendData8(USART1, TxBuffer[TxCounter++]);
USART_ClearITPendingBit(USART1, USART_IT_TC);
if(TxCounter == 10)
{
/* Disable the USART Transmit Complete interrupt */
USART_ITConfig(USART1, USART_IT_TC, DISABLE);
}
}USART_Cmd(USART1, DISABLE);
USART_ITConfig(USART1, USART_IT_TC, ENABLE);
USART_Cmd(USART1, ENABLE);call this to send data
USART MODE
[20:41:57.432]ÊÕ¡û¡ôþ
\0\06\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0
[20:41:57.469]ÊÕ¡û¡ô\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0
[20:41:57.505]ÊÕ¡û¡ô\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0
[20:41:57.542]ÊÕ¡û¡ô\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0
[20:41:57.579]ÊÕ¡û¡ô\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0
[20:41:57.615]ÊÕ¡û¡ô\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0ÿ\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0
[20:41:57.652]ÊÕ¡û¡ô\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0\0