STM8AL318A PORT I EXTI registers mapping
Hello
I am using stm8al318a lqfp80 package with GPIO pins PI0 - PI3.
The datasheet says 'all IOs mappable to interupt vectors' and the pin description has a check for ext. Interrupt.
But when reading reference manual RM0031 and the interrupt controller chapter with the EXTI registers specified, there are no bits in the registers mapping PORT I to interrupt vectors. There is a note in chapter 12.6 saying 'Port G, H and I are available on medium+ and high-density devices only'
My question is how can I map a GPIO on for example PI2 to an external interrupt?
/Johan