Question
STM8L DISCOVERY I2C
Posted on March 19, 2013 at 20:55
Hello all STM comunity,
First of all my apologies for my English, my language level is rather basic yet. That said, I will proceed to explain te reasons as I am writing this post.I am a Spanish estudent and I am developing a proyect with the demo board stm8l discovery. For this proyect I need to comunicate the MCU with an external ADC, becouse I need a 18-bit resolution.So I am trying to comunicate STM8L DISCOVERY (master) with MCP3424 (Slave).Folowing I2C protocol, at first I check that the I2C bus is not busy anymore and next, I send the start condition. The problem is that after I send the start condition, SDA goes low (that its correct) but SCL goes lo too and no clock signal is generated, SCL is low level constantly.I have tried to change the I2C bus frecuency, the pull up resistor are correct, and the chip is not borken. The start condition function that I´m using as follows: /* This function issues a start condition and * transmits the slave address + R/W bit * * Parameters: * I2Cx --> the I2C peripheral e.g. I2C1 * address --> the 7 bit slave address * direction --> the tranmission direction can be: * I2C_Direction_Tranmitter for Master transmitter mode * I2C_Direction_Receiver for Master receiver */void I2C_start(I2C_TypeDef* I2Cx, uint8_t address, uint8_t direction){ // wait until I2C1 is not busy anymore while(I2C_GetFlagStatus(I2Cx, I2C_FLAG_BUSY)); // Send I2C1 START condition I2C_GenerateSTART(I2Cx, ENABLE); // wait for I2C1 EV5 --> Slave has acknowledged start condition while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_MODE_SELECT)); // Send slave Address for write I2C_Send7bitAddress(I2Cx, address, direction); /* wait for I2C1 EV6, check if * either Slave has acknowledged Master transmitter or * Master receiver mode, depending on the transmission * direction */ if(direction == I2C_Direction_Transmitter){ while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED)); } else if(direction == I2C_Direction_Receiver){ while(!I2C_CheckEvent(I2Cx, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED)); }}The function is waiting ack after send the slave adrees, is obvious, beouse it is not clock. (I have measured whit an oscilloscope).I would be ver grateful if someone trying to help me.Greetings from Spain,Juan Cristóbal