STM8L050J3 SON8N - how to generate PWM on PC5 ?
Hello,
I am trying to generate a PWM signal on pin PC5 using TIM2_CH1 , but no success. But I am able to generate PWM on pin PD0 using TIM3_CH2.
Normally the procedure is quite simple :
for TIM2_CH1 - pin PC5
TIM2_OC1Init(TIM2_OCMode_PWM1, TIM2_OutputState_Enable,
DutyCycleValue,
TIM2_OCPolarity_High, TIM2_OCIdleState_Reset);
TIM2_OC1PreloadConfig(ENABLE);
TIM2_ARRPreloadConfig(ENABLE);
TIM2_CtrlPWMOutputs(ENABLE);
TIM2_Cmd(ENABLE);
But I see no PWM on pin PC5.
After searching in the RM0031 Reference manual I found this :
11.5.3 SYSCFG remap control register 3 (SYSCFG_RMPCR3)

So it appears the TIM2_CH1 can't be mapped on PC5 in STM8L with 8 pins ?
Because in STM8L050J3 datasheet it seems the function is supported

When I use a similar procedure on TIM3_CH2 there is a PWM on pin PD0
TIM3_OC2Init(TIM3_OCMode_PWM1, TIM3_OutputState_Enable,
DutyCycleValue,
TIM3_OCPolarity_High, TIM3_OCIdleState_Reset);
TIM3_OC2PreloadConfig(ENABLE);
TIM3_ARRPreloadConfig(ENABLE);
TIM3_CtrlPWMOutputs(ENABLE);
TIM3_Cmd(ENABLE);
Thank you,
Stefan