Skip to main content
Visitor II
May 18, 2020
Question

STM8L051 125khz PWM not work

  • May 18, 2020
  • 0 replies
  • 681 views

I have new application used stm8l051, The MCU using timer2(GPIOB2) to generator 125khz PWM, duty cycle from 0% to 100% every 500ms with 16Mhz clock source.

void Timer2_PWM_Init(void)

{

 GPIO_Init(GPIOB, GPIO_Pin_2, GPIO_Mode_Out_PP_High_Fast); 

 CLK_PeripheralClockConfig(CLK_Peripheral_TIM2,ENABLE);  

 TIM2_DeInit();                                              

 TIM2_TimeBaseInit(TIM2_Prescaler_1, TIM2_CounterMode_Up, 127);       // 16MHz clock source, 125kHz    

 TIM2_OC1Init(TIM2_OCMode_PWM2, TIM2_OutputState_Enable, 0, TIM2_OCPolarity_Low, TIM2_OCIdleState_Set);  

 TIM2_Cmd(ENABLE);                                          

}

void Timer2_PWM_SetDutyCycle(U8 Timer2_PWM_DutyCycle)

{

 TIM2_SetCompare1(127*Timer2_PWM_DutyCycle/100); 

}

This code is not working when generator 125Khz, but I did change output to 10khz it is work well, I attached the picture.I don't know reason of MCU. I have try with stm32f070 result is same.

    This topic has been closed for replies.