stm8l151c8 Interrupt is not working
Hi,
I'm using stm8l151c8 controller, I'm trying to get an interrupt from PB0 but it's not working, here is my code:
&sharpinclude 'stm8l15x_conf.h'
&sharpinclude 'main.h'
uint8_t __IO BlinkSpeed = 0;
static __IO uint32_t TimingDelay;void Delay(__IO uint32_t nCount)
{ while(nCount--) { }}void TimingDelay_Decrement(void)
{ if (TimingDelay != 0x00) { TimingDelay--; }}uint8_t data_audio,data_transmit;
uint8_t get_bit(uint8_t bits, uint8_t pos)
{ return (bits >> pos) & 0x01;}&sharppragma vector=0x008028
@svlreg @interrupt void EXTI0_IRQHandler()
{uint8_t i=0; if (EXTI_GetITStatus(EXTI_IT_Pin0) != RESET) {Delay(3); for(i=0;i<8;i++) { data_audio=data_audio<<0x01; data_audio=data_audio|GPIO_ReadInputDataBit(GPIOB,GPIO_Pin_0); Delay(5); } for(i=0;i<8;i++) { data_transmit=get_bit(data_audio,7-i); if(data_transmit==0x00) GPIO_WriteBit(GPIOD,GPIO_Pin_2,0x00); else GPIO_WriteBit(GPIOD,GPIO_Pin_2,0x01); Delay(10); } // Clear interrupt flag EXTI_ClearITPendingBit(EXTI_IT_Pin0); } }void GPIO_cnfg(){ GPIO_Init(GPIOD,GPIO_Pin_2,GPIO_Mode_Out_PP_Low_Fast); GPIO_Init(GPIOB,GPIO_Pin_0,GPIO_Mode_In_FL_IT); EXTI_SelectPort(EXTI_Port_B); EXTI_SetHalfPortSelection(EXTI_HalfPort_B_LSB, ENABLE); EXTI_SetPortSensitivity( EXTI_Port_B, EXTI_Trigger_Rising); EXTI_SetPinSensitivity(EXTI_IT_Pin0, EXTI_Trigger_Rising); enableInterrupts();}static void CLK_Config(void){ /* Select HSE as system clock source */ CLK_SYSCLKSourceSwitchCmd(ENABLE); CLK_HSICmd(ENABLE); CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI); /* system clock prescaler: 1*/ CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1); while (CLK_GetSYSCLKSource() != CLK_SYSCLKSource_HSI) {}}
int main (void) {CLK_Config();
GPIO_cnfg();
while(1) {
}}&sharpifdef USE_FULL_ASSERT
void assert_failed(uint8_t* file, uint32_t line){while (1)
{ }}&sharpendifand here is stm8_interrupt_vector.c
&sharpinclude 'main.h'
typedef void @far (*interrupt_handler_t)(void);
struct interrupt_vector {
unsigned char interrupt_instruction; interrupt_handler_t interrupt_handler;};@far @interrupt void NonHandledInterrupt (void)
{ return;}extern void _stext(); /* startup routine */
extern void EXTI0_IRQHandler();struct interrupt_vector const _vectab[] = {
{0x82, (interrupt_handler_t)_stext}, /* reset */ {0x82, NonHandledInterrupt}, /* trap */ {0x82, (interrupt_handler_t)EXTI0_IRQHandler}, /* irq0 */ {0x82, NonHandledInterrupt}, /* irq1 */ {0x82, NonHandledInterrupt}, /* irq2 */ {0x82, NonHandledInterrupt}, /* irq3 */ {0x82, NonHandledInterrupt}, /* irq4 */ {0x82, NonHandledInterrupt}, /* irq5 */ {0x82, NonHandledInterrupt}, /* irq6 */ {0x82, NonHandledInterrupt}, /* irq7 */ {0x82, NonHandledInterrupt}, /* irq8 */ {0x82, NonHandledInterrupt}, /* irq9 */ {0x82, NonHandledInterrupt}, /* irq10 */ {0x82, NonHandledInterrupt}, /* irq11 */ {0x82, NonHandledInterrupt}, /* irq12 */ {0x82, NonHandledInterrupt}, /* irq13 */ {0x82, NonHandledInterrupt}, /* irq14 */ {0x82, NonHandledInterrupt}, /* irq15 */ {0x82, NonHandledInterrupt}, /* irq16 */ {0x82, NonHandledInterrupt}, /* irq17 */ {0x82, NonHandledInterrupt}, /* irq18 */ {0x82, NonHandledInterrupt}, /* irq19 */ {0x82, NonHandledInterrupt}, /* irq20 */ {0x82, NonHandledInterrupt}, /* irq21 */ {0x82, NonHandledInterrupt}, /* irq22 */ {0x82, NonHandledInterrupt}, /* irq23 */ {0x82, NonHandledInterrupt}, /* irq24 */ {0x82, NonHandledInterrupt}, /* irq25 */ {0x82, NonHandledInterrupt}, /* irq26 */ {0x82, NonHandledInterrupt}, /* irq27 */ {0x82, NonHandledInterrupt}, /* irq28 */ {0x82, NonHandledInterrupt}, /* irq29 */};main.h file includes only the prototype of the interrupt function:
@svlreg @interrupt void EXTI0_IRQHandler();
every time it calls nonhandled interrupt function, but the address I'm putting in pragma vector line is correct, it's weird, I guess there is something missing.
Thank you for your help.
#stm8s-interrupt #interrupt #interrupt-issue