Question
STM8L152C6T6 USART1 Interrupt mode
Posted on January 13, 2015 at 08:22
Hi,
I am trying to transfer and read data from USART1 in interrupt mode but failed to do so. I successfully communicated with the polled method. I am not able to run any interrupt.No interrupt is executed as I write in ISR to on led but not reached to interrupt handler. that means inerrupt is not executed.My codes arevoid USART_init(unsigned int BaudRate);void USART_Tx_Buffer(char *Str);main(){ DeInitClock(); DeInitGPIO(); /* Select HSI as system clock source */ &sharpifdef USE_HSI CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI); CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1); &sharpelse CLK_SYSCLKSourceSwitchCmd(ENABLE); /* Select 2MHz HSE as system clock source */ CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSE); CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_4); CLK_HSICmd(DISABLE); &sharpendif RS232_ON(); UART_PORT_PIN_HIGH(); USART_init(9600); enableInterrupts(); USART_Tx_Buffer(''t'');}void USART_init(unsigned int BaudRate){ USART_Cmd(USART1,ENABLE); USART_DeInit(USART1); CLK_PeripheralClockConfig(CLK_Peripheral_USART1, ENABLE); USART_Init(USART1,BaudRate,USART_WordLength_8b,USART_StopBits_1,USART_Parity_No,USART_Mode_Tx|USART_Mode_Rx); USART_ClockInit(USART1,USART_Clock_Enable,USART_CPOL_Low, USART_CPHA_1Edge,USART_LastBit_Disable); USART_ReceiverWakeUpCmd(USART1,SET); USART_ITConfig(USART1,USART_IT_RXNE|USART_IT_TXE,ENABLE); }void USART_Tx_Buffer(char *Str){ char Str_Length=0,i=0; Str_Length=strlen(Str); for(i=0;i<=Str_Length;i++) { while(USART_GetFlagStatus(USART1,USART_FLAG_TXE) == RESET); USART_SendData8(USART1,*Str++); while (USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET); //Rx_Data_Buffer[i] = USART_ReceiveData8(USART1); } }In stm8it.c fileINTERRUPT_HANDLER(USART1_RX_IRQHandler,28){/* In order to detect unexpected events during development, it is recommended to set a breakpoint on the following instruction.*/ //while (1); portB_led=ON;} #stm8l152c6t6-usart1-interrupt-mo