STM8S-Discovery I2C problems
I have the problem with I2C comunication.
I programmed two STM8S-Discovery with example firmware available in C:\Users\u.iaquinta\Downloads\en.stsw-stm8069\STM8S_StdPeriph_Lib\Project\STM8S_StdPeriph_Examples\I2C\I2C_TwoBoards\I2C_DataExchange
One discovery is master and the second discovery is slave.

Rp1 and Rp2 is 10 K.
The interrupt I2C not start.
The master firmware is:
void main()
{/* system_clock / 1 */
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);/* I2C Initialize */
I2C_Init(I2C_SPEED, 0xA0, I2C_DUTYCYCLE_2, I2C_ACK_CURR, I2C_ADDMODE_7BIT, 16);/* Enable Buffer and Event Interrupt*/
I2C_ITConfig((I2C_IT_TypeDef)(I2C_IT_EVT | I2C_IT_BUF) , ENABLE);enableInterrupts();
.......
.......
........
}
Any idea?
Thanks