Question
STM8S TIM1 PWM2 not working
Posted on June 25, 2016 at 05:22
Hi all. please help me. I program my code in IAR embeded, I built no error, no warning, but it not working. this is my code in main.c :
#include ''main.h''void main(void){ CLK_HSICmd(ENABLE); CLK_SYSCLKConfig(CLK_PRESCALER_HSIDIV1); GPIO_Config(); TIM1_Config(); while (1) {//TIM1_SetCompare1(349); } }void TIM1_Config(){ TIM1_DeInit(); /* cau hinh timer 1 co dau ra PWM la 10kHz - bo chia tan 2 - duty =30% Ftimer=16/2=8Mhz TimerPeriod= Ftimer/Fpwm -1=799 */ TIM1_TimeBaseInit(1, TIM1_COUNTERMODE_UP, 799, 0); TIM1_SelectOCxM(TIM1_CHANNEL_1,TIM1_OCMODE_PWM2); TIM1_OC1PolarityConfig(TIM1_OCPOLARITY_LOW); TIM1_CCxCmd(TIM1_CHANNEL_1,ENABLE); TIM1_SetCompare1(239); TIM1_OC1PreloadConfig(ENABLE); TIM1_ARRPreloadConfig(ENABLE); /* TIM1 counter enable */ TIM1_Cmd(ENABLE); /* TIM1 Main Output Enable */ TIM1_CtrlPWMOutputs(ENABLE); }void GPIO_Config(void){ GPIO_DeInit(GPIOB); GPIO_Init(GPIOB,GPIO_PIN_5,GPIO_MODE_OUT_PP_LOW_FAST); GPIO_DeInit(GPIOC); GPIO_Init(GPIOC,GPIO_PIN_6,GPIO_MODE_OUT_PP_LOW_FAST);}and my code in main.h #ifndef __MAIN_H#define __MAIN_H/* Includes ------------------------------------------------------------------*/#include ''stm8s.h''#include ''user_delay.h''void TIM1_Config();void GPIO_Config(void);#endif /* __MAIN_H */ thanks for helping!