STM8S001J3 Locked After Configuring SWIM Pin as GPIO
Hello STM Community,
I am working with the STM8S001J3 microcontroller and facing an issue with configuring the SWIM pin (PD1) as a GPIO for LED control.
Here is the problem:
- When I configure the SWIM pin as a GPIO, the MCU gets locked, and I am unable to download any code into the microcontroller afterward.
- To mitigate this, I tried adding a delay before configuring the SWIM pin as GPIO, but the issue persists — the MCU still gets locked.
Is there a proper way to configure the SWIM pin as GPIO and still retain the ability to program the MCU afterward?
If before the I/O configure disable SWIM mode then I configure SWIM pin as I/O (GPIO) pin and after power reset swim mode enable or disable ?
Thank you in advance.