STM8S001J3M3 pull-up resistor value on PB4
In an application we use PB4 as output. Corresponding to the datasheet, this port only can be used with open-drain. In the datasheet in the I/O port pin characteristics there are values of 30k up to 80k for pull-up resistor Rpu. Is this meant for the internal pull up resistor?
I put 10k up to 3.3V. And with this value, I only get about 2.7V as high. If I put 30k, there will only be about 2V.
So, what are the usual values you put on these o.d ports on STM8?