Question
STM8S003 125khz PWM not work
Posted on May 29, 2016 at 11:50
Hi All,
I have new application used STM8S003, The MCU using timer1 or timer2 to generator 125khz PWM, duty cycle is 50% with 8Mhz HSI clock source.- This is my code to initial time2:static void Timer2_Init(void){ //Reset value: TIM2_DeInit(); //Config clock for timer2: //timer freq = (clock CPU/8) -> 1bit = 1uS -> 8*1uS=8uS (125khz). TIM2_TimeBaseInit(TIM2_PRESCALER_8,8); /* PWM1 Mode configuration: Channel1 */ TIM2_OC1Init(TIM2_OCMODE_PWM2, TIM2_OUTPUTSTATE_ENABLE,500, TIM2_OCPOLARITY_HIGH); TIM2_OC1PreloadConfig(ENABLE); TIM2_ARRPreloadConfig(ENABLE); TIM2_Cmd(ENABLE); }- System clock init:static void System_init(void){ CLK_DeInit(); CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1);//CPU Prescaler = 1/ CLK_SYSCLKConfig(CLK_PRESCALER_HSIDIV2);//Prescaler = 8, 16Mhz //CLK_CCOCmd(ENABLE); CLK_CCOConfig(CLK_OUTPUT_CPUDIV64);//Output clock on CCO pin. CLK_ClockSwitchConfig( CLK_SWITCHMODE_AUTO,//Enable the automatic clock switching mode CLK_SOURCE_HSI ,//Clock Source HSI. DISABLE , //Disable interrupt CLK_CURRENTCLOCKSTATE_DISABLE//Current clock enable ); CLK_PeripheralClockConfig (CLK_PERIPHERAL_TIMER1,ENABLE); CLK_PeripheralClockConfig (CLK_PERIPHERAL_TIMER2,ENABLE); CLK_PeripheralClockConfig (CLK_PERIPHERAL_TIMER4,ENABLE); //HSI Presscaler (1,2,4,8) //CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);//Setting 16Mhz. CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV2);//Setting 8Mhz. //CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV4);//Setting 4Mhz. //CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV128);//Setting 125khz. //While until HSI is ready! while(CLK_GetFlagStatus(CLK_FLAG_HSIRDY)!=SET);}This code is not working when generator 125Khz, but I did change output to 3khz it is work well, I don't know reason of MCU. I have try with timer1 result is same.Please help me to review my code and help me to fix that.Thanks #pwm125k-with-stm8s