Skip to main content
Visitor II
July 18, 2019
Question

STM8S003 program disappears

  • July 18, 2019
  • 0 replies
  • 456 views

I am currently using STM8S003 and use to option byte

During normal use, sometimes the program suddenly disappears.

Then when re-burn, it will fail and the following message will show:

Errors while setting configuration with MCU name STM8S103F3P: gdi-error [40701]: Option bytes read error

I don't know if it is a problem with the MCU itself or with my circuit?

(Vcc = 3V / with internal oscillator)

    This topic has been closed for replies.