STM8S003F3 - flash endurance and lab classes
Hello,
The STM8S003F3 is a Value Line device with quite small number of write/erase cycles. The data sheet says:
Program memory: 8 Kbyte Flash memory; data retention 20 years at 55 °C after 100 cycles
---
My wife is going to use very cheap W1209 thermostat module for lab classes in her school. This module based on STM8S003F3 has 7-segment display, buttons, led, relay, temperature sensor.
----
What makes me thinking is the small number of write/erase cycles.
Assuming that the required minimum data retension is a few weeks (maximum period between classes) - how many write/erase cycle is expected for the STM8S003F3 in the room temperature?
Thanks,
Bogdan