Question
STM8S003F3 & GPIOA
Posted on January 19, 2012 at 10:27
Hello.
I am new for this CPU. I use the discovery board to test my SW.I use 3 pin on GPIOA pin 1 2 and 3:GPIO_Init(THRUSTER_STATE, BOW_STATE , GPIO_MODE_IN_PU_IT); // PullUp input with interruptGPIO_Init(THRUSTER_STATE, STERN_STATE , GPIO_MODE_IN_PU_IT); // PullUp input with interruptGPIO_Init(RF_BUTTON_PORT, RF_BUTTON_PIN , GPIO_MODE_IN_PU_IT); // PullUp input with interruptEXTI_SetExtIntSensitivity(EXTI_PORT_GPIOA, EXTI_SENSITIVITY_FALL_ONLY); pull-up is okbut when I run debugg it seam at interrupt work low only? Why I have done wrong? and it seans at pin 1 of GPIOA not working.. perhaps it used on this board already.Thierry #stm8s-discovery