STM8S003F3 VIH and VIL levels
Hello all,
I have an application based on the STM8S003F3 where invalid logic levels could appear on the UART RX line. (By design due to the ground offsets in a bigger system.) In some cases the UART misinterprets bytes mainly when the low level of the 0 bits is around 2.2V
In the DS7147 page 66 section 9.3.6 the following is present:

My application uses 5V VDD, so if I calculate right the VIHmin is 3.5V and the VILmax is 1.5 V in my case.
And in the following page there is a graph which is the following:
If I read it right the VIL is ~2.2V and the VIH is ~2.9V.
Which is the correct one?