STM8S005K6 I2C Bus always busy
Hi.
Regarding I2C Bus busy problem.
I am using alternative pins (PB4 and PB5), as I have the small chip with fewer pins.
Option bits are set, and verified.
However even at power up the BUSY bit is set. It is set through configuration of the I2C peripheral.
It is cleared when I active SWRST bit, but as soon as I clear it, BUSY is set again.
Is there a problem using alternative pins (or do I need to do something further than setting the option bit)?