Skip to main content
Visitor II
January 21, 2025
Question

STM8S103 Code Upload / Execution Issue

  • January 21, 2025
  • 2 replies
  • 2030 views

Issue with STM8S103 Code Uploading on Identical PCB Boards

I have two identical PCB boards, both equipped with the STM8S103 microcontroller. One board functions perfectly, with code uploading and running as expected, while the other does not.

Observations

  1. Voltage Measurements

    • On the non-working board:
      • NRST pin: 1.6V
      • SWIM pin: 3.2V
    • On the working board:
      • NRST pin: 3.2V
      • SWIM pin: Floating around 200mV
  2. Microcontroller Replacement

    • Suspecting a defective STM8S103 on the non-working board, I desoldered it and placed it on a functioning development board (See the attachement).
    • To my surprise, the board started working perfectly—code uploaded and executed without issues.
    • I measured the voltage on the NRST and the SWIM pins. which were same as in the working board mentioned above.
    • This indicates that the microcontroller on the non-working board is not faulty.

Setup

  • Development Tools:
    • SDUINO
    • Arduino IDE
    • ST LINK V2

I would greatly appreciate any insights or suggestions to identify the root cause of this issue 

Thank you!

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    January 21, 2025

    Welcome @SuwinManudewa, to the community!

    As you have already described, there was either a problem with the board where you soldered down the apparently faulty STM8S, or the programming went wrong beforehand. I suspect the former, as I've seen quite a few boards with invisible shorts and other issues.

    In this context: is your ST-LINK/V2 one of those fakes in a colourful tin can?

    Regards
    /Peter

    Visitor II
    January 23, 2025

    is there perticular reason the STM8S103's NRST pin goes to 1.6V and the SWIM pin to 3.2V???

    Graduate II
    January 23, 2025

    Badly soldered, improper orientation. If the parts Ok on a simpler board, review your PCB, check nets and components placed.

    Two drivers attempting to drive in different states? Anything programmed on to the IC?

    Is this a DC voltage, or oscillating level?

    Technical Moderator
    January 23, 2025

    I am not aware of any reason for this.

    Will you also answer my question?