Skip to main content
Explorer
October 12, 2023
Question

STM8S103F3 programming error while using STVP

  • October 12, 2023
  • 1 reply
  • 1590 views

Hi All,

This is my first post here and also my first interaction with ST micro devices

I'm truing to flash a .hex file into an STM8S103F3 using ST LINK V2 and STVP but I cannot connect to the device. I'm using a 5V external supply connected to the VDD and GND of the IC and ST Link and the SWIM and Reset wires are connected to pin 18 and 4. I have initially tried this on our product but I need to try to flash the device offline and I'm struggling to find a solution. Tried 3.3V as well, tried without the external supply, tried with different devices and multiple ST Link programmers. Same result. STVP has been set up correctly, with ST Link, SWIM and the correct device.

Is there anything I'm missing?

Thanks for your support!

IMG_4109.JPGIMG_4110.JPGCapture.PNG

    This topic has been closed for replies.

    1 reply

    Graduate II
    October 12, 2023

    Check voltages, add VCAP

    gabriel86Author
    Explorer
    October 13, 2023

    Fitted a 100nF cap and not it works 

    Much appreciated :)