structure @0xXXXX
I am trying to create a bit structure at a specified location (in this case at 0x500A the portc odr)
below is in common.h
struct iobits
{unsigned char b0:1;unsigned char b1:1;unsigned char b2:1;unsigned char b3:1;unsigned char b4:1;unsigned char b5:1;unsigned char b6:1;unsigned char b7:1;};extern struct iobits oportc;and this is in the main.c file
at 0x500A struct iobits oportc;
This works with Raisonance compiler, but not the Cosmic.
I then read that the Cosmic needed the following format
struct iobits oprotc @0x500A;
However an error occurs as follows:-
#error clnk Debug\lcc.lkf:1 bad address (0x500a) for zero page symbol _oportc
If I declare it without absolute address or another variable with the same format it works.
In common.h
extern struct iobits oportc;
extern oportd;and in main.c
struct iobits oportc;
oportd @0x500A; void main(void){oportd = 0x55; // this is located at 0x500A
op_str = 1; // this is located in page zero.Any help would be most appreciated.