Skip to main content
Visitor II
March 26, 2011
Question

STVD displays ''The parameter is incorrect''

  • March 26, 2011
  • 35 replies
  • 5865 views
Posted on March 26, 2011 at 04:17

Just received my STM8L-Discovery, installed STVD 4.2.1 and Raisonance compiler. Whenever I hit F7, STVD shows this non-descriptive message ''The parameter is incorrect''. After that, the only way to exit the application is to kill it in the Task Manager. I tried it on Win XP and Win 7 (32-bit) with same results.

Does anyone experienced a similar problem?

Thanks for help!

    This topic has been closed for replies.

    35 replies

    Visitor II
    May 24, 2011
    Posted on May 24, 2011 at 10:17

    Hi,

     The patch is now ok and the delivery on ST site will be available end of this week (worst case).

    Best regards

    Phil

    Visitor II
    May 30, 2011
    Posted on May 30, 2011 at 10:19

    Hi 

     The patch#2 (for the toolset pack 24) for fix the problem ''The parameter is incorrect'' is available on link :

    http://www.st.com/internet/evalboard/product/210567.jsp

    Rgds

    Phil

    Visitor II
    May 30, 2011
    Posted on May 30, 2011 at 23:08

    Thanks!

    i've this problem and solved with your patch.

    Visitor II
    July 25, 2011
    Posted on July 25, 2011 at 13:33

    I've installed V4.2.1 and Patch 2 but still struggling with this problem of ''The parameter is incorrect'' on an ST8 application using the Assembler / Linker toolchain.

    I've tried to run the ST7 example 'realtime' supplied and this will not work either.

    The system loads the mapping.asm and main.asm automatically and when a build is attempted the system reports

       ST Visual Develop

    The executable could not be found

    You can fix it by editing your toolset settings etc. etc.

    It hangs up while attempting to assemble mapping.asm  and reports

    Error creating process for executable asm

    The parameter is incorrect

    Failed to create process.

    All files ie assembler, linker etc are located in a single project file and this is the path shown in project settings.

    Any idea what's going on and how I can work round it?

    Visitor II
    August 5, 2011
    Posted on August 05, 2011 at 21:59

    I've installed V4.2.1 and Patch 2 but still struggling with this problem of ''The parameter is incorrect'' on an ST8 application using the Assembler / Linker toolchain.

    I've tried to run the ST7 example 'realtime' supplied and this will not work either.

    The system loads the mapping.asm and main.asm automatically and when a build is attempted the system reports

       ST Visual Develop

    The executable could not be found

    You can fix it by editing your toolset settings etc. etc.

    It hangs up while attempting to assemble mapping.asm  and reports

    Error creating process for executable asm

    The parameter is incorrect

    Failed to create process.

    All files ie assembler, linker etc are located in a single project file and this is the path shown in project settings.

    Any idea what's going on and how I can work round it?