I am having difficulties in implementing a PWM for one output in TIM1 and making a time base generation in TIM2. (STM8S105K6) Regarding the TIM2: I want to have an internal 1920Hz signal without using the output pins. If I understood the refence manual correctly, that is possible by setting the counter clock in 16MHz(TIM2_PRESCALER_1) and counting until 8332 (16MHz/8332 = 1920.3Hz). So, by the end of each counting, I want the UPDATE interrupt to be generated so I can work with this time base. The following way is not working: TIM2_DeInit(); TIM2_TimeBaseInit(TIM2_PRESCALER_1,8332); TIM2_OC2Init(TIM2_OCMODE_INACTIVE, TIM2_OUTPUTSTATE_DISABLE,8332, TIM2_OCPOLARITY_HIGH); TIM2_OC2PreloadConfig(DISABLE); TIM2_ARRPreloadConfig(ENABLE); TIM2_ITConfig(TIM2_IT_UPDATE, ENABLE); TIM2_Cmd(ENABLE); enableInterrupts(); Now, talking about the PWM in TIM1, what is the correct way to configure a center-aligned counter with update event each underflow (TIM1_RCR = 1??)with frequency of 120Hz and amplitude of 1024? I thought this way: 2047 counts for each 120Hz(8.334ms), so if I use the 16MHz clock, the period would be: (8.3334e-3/2048)/(1/16e6) = 65 But the following way is not working also: (for duty cycle 0.5) TIM1_DeInit(); TIM1_TimeBaseInit(0, TIM1_COUNTERMODE_CENTERALIGNED1, 65,0); TIM1_OC1Init(TIM1_OCMODE_PWM1, TIM1_OUTPUTSTATE_ENABLE, TIM1_OUTPUTNSTATE_DISABLE, 65, TIM1_OCPOLARITY_LOW, TIM1_OCNPOLARITY_HIGH, TIM1_OCIDLESTATE_SET, TIM1_OCNIDLESTATE_RESET); TIM1_SetCompare1(512); TIM1_Cmd(ENABLE); TIM1_CtrlPWMOutputs(ENABLE); enableInterrupts(); It should not be that difficult, right? Thank you, Guilherme