TIM2 program using STM8S003F3
Hi
I am facing problem in Timer2 programing. It does not go into the interrupt. Please find below program of Timer2 initialization. I am using STVD for programing STM8S003F3.
The Prescalar clock frequency is 16Mhz
//Configuring TIM2 for 1 ms delay generation
TIM2->PSCR =0x04; //Deviding incoming clock by 16 Fck_cnt = Fck_psc/(2^PSC[3:0]); TIM2->ARRH =0x03; //ARR value with 1000 TIM2->ARRL =0xE8;TIM2->CR1 |= 0x80; //Auto reload preload enabled
TIM2->IER |=0x01; //TIM2 Update Interrupt enabled
TIM2->CR1 |= 0x01; //ON timerInterrupt routine as below in which PD6 is toggled on each interrrupt.
INTERRUPT_HANDLER(TIM2_UPD_OVF_BRK_IRQHandler, 13)
{ GPIOD->ODR ^=0x40; TIM2->SR1 &= 0xfe; //*/}
I am not getting what is wrong. Thanks in advance.