Question
TIM3 wrong counting?
Posted on September 04, 2012 at 17:14
I need to generate a 20 ms interrupt into my firmware. HSE is 16 Mhz with STM8S208.
I put this initialization code into my firmware to accomplish that through the use of TIM3: #define PRESC TIM3_PRESCALER_32 uint16_t counter = 10000;//counter = counter / 4 * 3; //correction to run closer to a 20 ms period
TIM3_UpdateRequestConfig(TIM3_UPDATESOURCE_GLOBAL);
TIM3_TimeBaseInit(TIM3_PRESCALER_32, counter);
TIM3_UpdateDisableConfig(DISABLE);
TIM3_PrescalerConfig (PRESCALER_32, TIM3_PSCRELOADMODE_UPDATE);
TIM3_ARRPreloadConfig(ENABLE);
TIM3_ITConfig(TIM3_IT_UPDATE, ENABLE);
To achieve the desired 20 ms period I initialized the counter to 10000, so that (16 Mhz / 32 presc = 500 Khz) / 10000 = 50 Hz. Unfortunately the actual frequency is 75% of the expected one, so I need to uncomment the counter correction statement. Does someone why does this happen? Regards. Giorgio