Has any one had problems with external input clock mode2 ?
I am attempting to count pulses thru TIM_ETR with no luck. I have followed the suggested procedure exactly i.e. set ECE in TIM1_ETR and CEN in TIM1_CR1. The exact micro is the STM8S207C8T6. The timer runs ok when internal clock selected and I can see from trial sofware that the pulses are going to PB3/pin19. The frequency is easily less than master/4 Any one else had any issues or solutions?