Question
UART communication using STM8L discovery
Posted on August 23, 2015 at 08:54
Hi,
I am new to use STM8L controller.I am just trying to put Simple character on UART using STM8L discovery board.But I am failed to do this.Following is my code for this.void main(void){ u8 Data = 'N'; CLK_DeInit(); GPIO_DeInit(GPIOC); CLK_HSICmd(ENABLE); CLK_SYSCLKSourceConfig(CLK_RTCCLKSource_HSI); CLK_SYSCLKDivConfig(CLK_SYSCLKDiv_1); GPIO_ExternalPullUpConfig(GPIOA, GPIO_Pin_3, ENABLE); GPIO_ExternalPullUpConfig(GPIOA, GPIO_Pin_2, ENABLE); USART_DeInit(USART1); CLK_PeripheralClockConfig(CLK_Peripheral_USART1, ENABLE); USART_Init(USART1, 9600, USART_WordLength_8b, USART_StopBits_1, USART_Parity_No, USART_Mode_Tx | USART_Mode_Rx); USART_ClockInit(USART1, USART_Clock_Disable, USART_CPOL_Low, USART_CPHA_1Edge, USART_LastBit_Disable); USART_Cmd(USART1, ENABLE); while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET) // Wait for transmition to complete { } USART_SendData8(USART1, Data); GPIO_Init(GPIOC, GPIO_Pin_7, GPIO_Mode_Out_PP_High_Fast); // Init Blue LED// GPIO_Init(GPIOE, GPIO_Pin_7, GPIO_Mode_Out_PP_High_Fast); // Init Green LED /* Infinite loop */ while (1) { // Wait for transmition to complete { } USART_SendData8(USART1, Data); GPIO_SetBits(GPIOC, GPIO_Pin_7); delay_ms(1000); GPIO_ResetBits(GPIOC, GPIO_Pin_7); delay_ms(1000); }}I am using IAR workbetch for STM8 evolution version.