UART issue for reading 2 or more bytes length
I am having an issue with the UART1 communication between two devices (Computer and a STM8S208 board).
I implemented software in the computer that writes two bytes length of data to the STM8
• the first byte that acts as an identifier;
•the second byte was the data that I wanted to write at VLS memory,
However, at the STM8, only the first byte was read and twice, For instance, I sent the identifier 0x04 and the data 0x90, but only the byte 0x04 was read and stored in the buffer as: (0x04 , 0x04 ).
Now I am implementing it reading 1-byte lenght each time via a UART interruption, but I am afraid that it could let the firmware more prone to bugs, in case of the data, have the same value of the identifier byte - Some of my data are 2 bytes long + 1 byte for Identifier.
I believe that the best solution is to send it as one byte for identifier plus two bytes for data, altogether.
But how could I implement it or why only the first byte is being read repeatly?
Below are the functions for Receiving and Writing data in the STM8:
void UART1_ReceiveBytes(uint8_t * buf, uint8_t numberOfBytes)
{
while (numberOfBytes > 0){
*(buf++) = UART1_ReceiveData8();
numberOfBytes--;
}
}
void UART1_SendBytes(uint8_t *data, unsigned int numberOfBytes)
{
while (numberOfBytes > 0) {
UART1_SendData8(*data++);
numberOfBytes--;
while(UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET);
}
}UART Setup:
void UART1_setup(void)
{
UART1_DeInit();
UART1_Init( 9600,
UART1_WORDLENGTH_8D,
UART1_STOPBITS_1,
UART1_PARITY_NO,
UART1_SYNCMODE_CLOCK_DISABLE,
UART1_MODE_TXRX_ENABLE);
UART1_ITConfig(UART1_IT_RXNE_OR, ENABLE);
enableInterrupts();
UART1_Cmd(ENABLE);
}