Question
Unable to compile any of the example code...
Posted on June 03, 2010 at 14:48
Hi there,
Before I go mad and smash up the STM8s Discovery Board, could someone please help me get some basic code up and running, Grom did manage to get the PWM code to work on the unit after many attempts... All I require is some basic code to set up the Uart2 and transmit and recieve commands to and from hyperterminal, then all I require is to get the ADC to recieve an input from a thermister.... Nothing too complicated, but this is the only processor that I have never been able to get working straight from the box...