Skip to main content
Visitor II
October 9, 2017
Question

Understanding STM8 pipelining

  • October 9, 2017
  • 0 replies
  • 566 views
Posted on October 09, 2017 at 14:18

I’m trying to understand STM8 pipelining to be able to predict how much cycles my code will need.

(I already

https://stackoverflow.com/questions/46629607/understanding-stm8-pipelining

, but I figured this focum is probably the better audience).

I have this example, where I toggle a GPIO pin for 4 cycles each. Iffloopis aligned at 4byte-boundary + 3, the pin stays active for 5 cycles (i.e. one more than it should). I wonder why?

// Switches port D2, 5 cycles high, 4 cycles low void main(void) {  __asm  bset 0x5011, #2 ; output mode  bset 0x5012, #2 ; push-pull  bset 0x5013, #2 ; fast switching  jra _loop  .bndry 4  nop  nop  nop  _loop:  nop  bset 0x500f, #2  nop  nop  nop  bres 0x500f, #2  jra _loop  __endasm; }

A bit more context:

  • bset/bresare 4 byte instructions,nop1 byte.
  • Thenop/bset/bresinstructions take 1 cycle each.
  • Thejrainstruction takes two cycles. I think in the first cycle, the instruction cache is filled with the next 32bit value, i.e. in this case thenopinstruction only. And the 2nd cycle is actually just the CPU being stalled while decoding the next instruction.

So in cycles:

  1. bresclears the pin
  2. jra, pipeline flush,nopfetch
  3. nopdecode,bsetfetch
  4. nopexecute,bsetdecode, nextnopfetch
  5. bsetexecute sets the pin
  6. nop,bresfetch
  7. nop
  8. nop,bresdecode
  9. bresexecute clears the pin

According to this, the pin should stay LOW for 4 cycles and HIGH for 4 cycles, but it’s staying HIGH for 5 cycles.

In any other alignment case, the pin is LOW/HIGH for 4 cycles as expected.

I think, if the PIN stays high for an extra cycle that must mean that the execution pipeline is stalled after thebsetinstruction (thenops thereafter provide enough time to make sure thatbreslater is ready to execute immediately). But according to my understandingnop(for 6.) would already be fetched in 4.

Any idea how this behavior can be explained? I couldn’t find any hints in the

http://www.st.com/content/ccc/resource/technical/document/programming_manual/43/24/13/9a/89/df/45/ed/CD001617pdf/files/CD001617pdf/jcr:content/translations/en.CD001617pdf

.

#cpu #cycle #pipelining #performance

    This topic has been closed for replies.